UF_MODL_parm_s (view source)
 
Defined in: uf_modl_types.h
 
Also known as:
 
Overview
The following structure is used to define input parameters
when there is an option between using a constant value or
a law.


Data Members

method_type
UF_MODL_parm_method_t
Indication of how the
parameter is being defined,
either through a constant
value, of which an expression
is made, or by a law.

defined_by
UF_MODL_parm_defined_by_union_t
Definition of the parameter