UF_MODL_offset_trans_faces_s
(view source)
Defined in: uf_modl_types.h
Also known as:
UF_MODL_offset_trans_faces_t
UF_MODL_offset_trans_faces_p_t
Data Members
faces
UF_MODL_faces_p_t
The faces to be offset or
translated.
method_type
UF_MODL_offset_trans_type_t
Indication of whether the faces
are to be offset or translated.
distance [ MAX_LINE_BUFSIZE ]
char
A character string containing the
constant value to offset or
translate the given faces.
direction
UF_MODL_vector_p_t
A vector defining the direction
of translation, only used if
method_type is
UF_MODL_TRANSLATION_OF_FACES. It
can be NULL otherwise.
translated.