UF_MODL_deviation_check_data_s (view source)
 
Defined in: uf_modl_types.h
 
Also known as:
 
Overview
Following is a structure definition for deviation checking.
It holds the output data of deviation checking.


Data Members

number_of_points_checked
int
Number of points checked

minimum_distance_error
double
Minimum distance deviation

maximum_distance_error
double
Maximum distance deviation

average_distance_error
double
Average distance deviation

minimum_angle_error
double
Minimum angle deviation

maximum_angle_error
double
Maximum angle deviation

average_angle_error
double
Average angle deviation

distance_errors
double *
Distance deviation at check points

angle_errors
double *
Angle deviations at check points

check_points) [ 3 ]
double (*
Points used in deviation checking