VisualReportSaveDestinationOption Enumeration¶
NXOpen.VisualReporting.VisualReport.SaveDestinationOption is an alias for NXOpen.VisualReporting.VisualReportSaveDestinationOption
-
class
NXOpen.VisualReporting.
VisualReportSaveDestinationOption
¶ Bases:
object
Represents the possible
NXOpen.VisualReporting.VisualReport.SaveDestination()
options for aNXOpen.VisualReporting.VisualReport
.Enum Members
Enum Member Enum Member Description Local Saves the report in the local file system.Teamcenter Saves the report in the Teamcenter database.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-