VisualReportReportingStyleOption Enumeration¶
NXOpen.VisualReporting.VisualReport.ReportingStyleOption is an alias for NXOpen.VisualReporting.VisualReportReportingStyleOption
-
class
NXOpen.VisualReporting.
VisualReportReportingStyleOption
¶ Bases:
object
Represents the possible
NXOpen.VisualReporting.VisualReport.ReportingStyle()
for aNXOpen.VisualReporting.VisualReport
.Enum Members
Enum Member Enum Member Description ColorObject Matching objects will be coloredTagObject Matching objects will be taggedColorAndTagObject Matching objects will be both colored and tagged-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-