VisualReportExplorerExploreReportOption Enumeration

NXOpen.VisualReporting.VisualReportExplorer.ExploreReportOption is an alias for NXOpen.VisualReporting.VisualReportExplorerExploreReportOption

class NXOpen.VisualReporting.VisualReportExplorerExploreReportOption

Bases: object

Represents whether Explore Report mode is on or off.

Enum Members

Enum Member Enum Member Description
Off
Explore Visual Report results is off
On
Explore Visual Report results is on
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.