VisualReportBuilderPropertyUsageOption Enumeration¶
NXOpen.VisualReporting.VisualReportBuilder.PropertyUsageOption is an alias for NXOpen.VisualReporting.VisualReportBuilderPropertyUsageOption
-
class
NXOpen.VisualReporting.
VisualReportBuilderPropertyUsageOption
¶ Bases:
object
Represents the usage option of reference
NXOpen.VisualReporting.Property
Enum Members
.
- . csv-table::
header: “Enum Member”, “Enum Member Description” “Tooltip”, “The property is used in tooltip only” “InfoView”, “The property is used in info view only” “TooltipAndInfoView”, ” - “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.