GroupLabelTagPriorityOption Enumeration

NXOpen.VisualReporting.GroupLabel.TagPriorityOption is an alias for NXOpen.VisualReporting.GroupLabelTagPriorityOption

class NXOpen.VisualReporting.GroupLabelTagPriorityOption

Bases: object

Represents the possible priority options for a NXOpen.VisualReporting.GroupLabel.

Enum Members

Enum Member Enum Member Description
Low
Low priority
Medium
Medium priority
High
Hign priority
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.