ConditionOperatorOption Enumeration

NXOpen.VisualReporting.Condition.OperatorOption is an alias for NXOpen.VisualReporting.ConditionOperatorOption

class NXOpen.VisualReporting.ConditionOperatorOption

Bases: object

Represents the possible operator type options.

for a NXOpen.VisualReporting.Condition.

Enum Members

Enum Member Enum Member Description
EqualOperator  
LessThanOperator  
NotLessThanOperator  
GreaterThanOperator  
NotGreaterThanOperator  
NotEqualOperator  
RegularExpressionOperator  
ContainsOperator  
DoesNotContainOperator  
OnOrBeforeOperator  
OnOrAfterOperator  
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.