ClassifierTypeOption Enumeration

NXOpen.VisualReporting.Classifier.TypeOption is an alias for NXOpen.VisualReporting.ClassifierTypeOption

class NXOpen.VisualReporting.ClassifierTypeOption

Bases: object

Represents the possible type options.

for a NXOpen.VisualReporting.Classifier.

Enum Members

Enum Member Enum Member Description
Simple
Simple classifier type
Value
Value classifier type
Range
Range classifier type
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.