ClassifierRangeMethodOption Enumeration

NXOpen.VisualReporting.Classifier.RangeMethodOption is an alias for NXOpen.VisualReporting.ClassifierRangeMethodOption

class NXOpen.VisualReporting.ClassifierRangeMethodOption

Bases: object

Represents the possible range method options.

for a NXOpen.VisualReporting.Classifier.

Enum Members

Enum Member Enum Member Description
Number
A numeric range will be used
Percentage
A percentage range will be used
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.