ClassifierGroupingMethodOption Enumeration¶
NXOpen.VisualReporting.Classifier.GroupingMethodOption is an alias for NXOpen.VisualReporting.ClassifierGroupingMethodOption
-
class
NXOpen.VisualReporting.
ClassifierGroupingMethodOption
¶ Bases:
object
Represents the possible grouping method options.
for a
NXOpen.VisualReporting.Classifier
.Enum Members
Enum Member Enum Member Description Manual Grouping is manualAutomatic Grouping is automaticSemiAutomatic Grouping is automatic but some :py:class:`NXOpen.VisualReporting.GroupLabel`s have been modified-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-