InstantiationBuilder Class
Properties
Property |
Description |
Explosion |
Returns or sets the property of whether user is allowed to explode User Defined Template instantiation |
LayerNumber |
Returns or sets the output layer number user specify for User Defined Template instantiation |
LayerOption |
Returns or sets the property of output layer option of User Defined Template instantiation |
Tag |
Returns the Tag for this object. |
Methods
Method |
Description |
Commit |
Commits any edits that have been applied to the builder. |
Destroy |
Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects |
For builders that create more than one object, this method returns the objects that are created by commit. |
GetExpressions |
Returns the expressions in User Defined Template @return |
GetMatchedExpression |
Returns the matched expression of an original expression in User Defined Template @return |
GetMatchedReference |
Returns the matched reference of an original reference in User Defined Template @return |
GetObject |
Returns the object currently being edited by this builder. |
GetReferences |
Returns the references in User Defined Template @return |
LoadAuthoringPart |
Return the authoring part of User Defined Template object @return |
SetMatchedReference |
Set the matched reference of an original reference in User Defined Template |
ShowResults |
Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate |
Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail
Explosion
LayerNumber
LayerOption
Method Detail
GetExpressions
GetMatchedExpression
GetMatchedReference
GetReferences
LoadAuthoringPart
SetMatchedReference
Validate