UserDefinedObjectDisplayContextViewMode Enumeration

NXOpen.UserDefinedObjects.UserDefinedObjectDisplayContext.ViewMode is an alias for NXOpen.UserDefinedObjects.UserDefinedObjectDisplayContextViewMode

class NXOpen.UserDefinedObjects.UserDefinedObjectDisplayContextViewMode

Bases: object

The enumerated view mode

Enum Members

Enum Member Enum Member Description
NotShaded
The view is not shaded
PartiallyShaded
The view is partially shaded
FullyShaded
The view is fully shaded
AnalysisShaded
The view is analysis shaded
StudioShaded
The view is studio shaded
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.