UserDefinedObjectDisplayContextStandardTextRef Enumeration

NXOpen.UserDefinedObjects.UserDefinedObjectDisplayContext.StandardTextRef is an alias for NXOpen.UserDefinedObjects.UserDefinedObjectDisplayContextStandardTextRef

class NXOpen.UserDefinedObjects.UserDefinedObjectDisplayContextStandardTextRef

Bases: object

This enumerated type specifies the type of reference point used in the text box for standard_text methods.

Enum Members

default reference point position “
“BaselineStart”, ” Display the text starting on the

baseline, at the left end of the text box for left-to-right text, or at the right end of the text box for right-to-left text “

“BaselineCenter”, ” Display the text with the given position

in the horizontal center of the text box at the baseline “

“BaselineEnd”, ” Display the text starting on the baseline,

at the right end of the text box for left-to-right text, or at the left end of the text box for right-to-left text “

“TopLeft”, ” Display the text with the given position
in the top left of the text box “
“TopCenter”, ” Display the text with the given position
in the top center of the text box “
“TopRight”, ” Display the text with the given position
in the top right of the text box “
“MiddleLeft”, ” Display the text with the given position
in the middle left of the text box “
“MiddleCenter”, ” Display the text with the given position
in middle center of text box “
“MiddleRight”, ” Display the text with the given position
in middle right of text box “
“BottomLeft”, ” Display the text with the given position
in bottom left of text box “
“BottomCenter”, ” Display the text with the given position
in bottom center of text box “
“BottomRight”, ” Display the text with the given position

in bottom right of text box “

ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.