UserDefinedObjectDisplayContextFacetType Enumeration

NXOpen.UserDefinedObjects.UserDefinedObjectDisplayContext.FacetType is an alias for NXOpen.UserDefinedObjects.UserDefinedObjectDisplayContextFacetType

class NXOpen.UserDefinedObjects.UserDefinedObjectDisplayContextFacetType

Bases: object

The enumerated type facet to be displayed

Enum Members

Enum Member Enum Member Description
Triangle
The facet topology is a triangle facet
Polygon
The facet topology is a polygon facet
Tristrip
The facet topology is a tristrip facet
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.