ToolPalette Class¶
-
class
NXOpen.UIStyler.
ToolPalette
¶ Bases:
NXOpen.UIStyler.StylerItem
Represents a ToolPalette for UI Styler
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
ItemValue | Returns or sets the currently selected choice for this dialog item. |
Visibility | Returns or sets the visibility of the dialog item |
Methods¶
Method | Description |
---|---|
AddActivateHandler | Registers activate callback. |
Dispose | Free resources associated with the instance. |
GetItemType | Gets the dialog item type. |
GetSensitivity | Gets the sensitivity of the dialog item @return True if sensitivity is set otherwise False |
InitializeAttachment | Returns initialized dialog item attachment information @return attachment object |
IsEqualTo | Equates two styler items @return |
SetAttachment | Specifies the updated dialog item attachment information |
SetDefault | Indicates that this dialog item should override the accelerator on the second mouse button, which normally accelerates to the OK button. |
SetLabel | Specifies descriptive text to display for the dialog item. |
SetSensitivity |
Property Detail¶
ItemValue¶
-
ToolPalette.
ItemValue
¶ Returns or sets the currently selected choice for this dialog item.
-------------------------------------
Getter Method
Signature
ItemValue()
Returns: Item value Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ItemValue(itemVal)
Parameters: itemVal (int) – Item value New in version NX5.0.0.
License requirements: None.
Visibility¶
-
ToolPalette.
Visibility
¶ Returns or sets the visibility of the dialog item
-------------------------------------
Getter Method
Signature
Visibility()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Visibility(type)
Parameters: type (bool) – New in version NX5.0.0.
License requirements: None.
Method Detail¶
AddActivateHandler¶
-
ToolPalette.
AddActivateHandler
¶ Registers activate callback.
This method should be called before calling
UIStyler.Dialog.Show()
orUIStyler.Dialog.RegisterWithUiMenu()
Signature
AddActivateHandler(activateevent, isDialogLaunchingEvent)
Parameters: - activateevent (CallableObject) –
- isDialogLaunchingEvent (bool) –
New in version NX5.0.0.
License requirements: None.
GetSensitivity¶
-
ToolPalette.
GetSensitivity
¶ Gets the sensitivity of the dialog item
Signature
GetSensitivity()
Returns: True if sensitivity is set otherwise False Return type: bool New in version NX5.0.0.
License requirements: None.
SetDefault¶
-
ToolPalette.
SetDefault
¶ Indicates that this dialog item should override the accelerator on the second mouse button, which normally accelerates to the OK button.
When you set this attribute, a click on the second mouse button triggers this dialog item’s Activate callback instead of the action of the OK button.
Signature
SetDefault(dialogId)
Parameters: dialogId (int) – New in version NX5.0.0.
License requirements: None.