ScrolledWindow Class¶
-
class
NXOpen.UIStyler.
ScrolledWindow
¶ Bases:
NXOpen.UIStyler.StylerItem
Represents a ScrolledWindow for UI Styler
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Sensitivity | Returns or sets |
Visibility | Returns or sets |
Methods¶
Method | Description |
---|---|
Dispose | Free resources associated with the instance. |
GetItemType | Gets the dialog item type. |
InitializeAttachment | Returns initialized dialog item attachment information @return attachment object |
IsEqualTo | Equates two styler items @return |
SetAttachment | Specifies the updated dialog item attachment information |
Property Detail¶
Sensitivity¶
-
ScrolledWindow.
Sensitivity
¶ Returns or sets
-------------------------------------
Getter Method
Signature
Sensitivity()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Sensitivity(type)
Parameters: type (bool) – New in version NX5.0.0.
License requirements: None.
Visibility¶
-
ScrolledWindow.
Visibility
¶ Returns or sets
-------------------------------------
Getter Method
Signature
Visibility()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Visibility(type)
Parameters: type (bool) – New in version NX5.0.0.
License requirements: None.