RealItem Class¶
-
class
NXOpen.UIStyler.
RealItem
¶ Bases:
NXOpen.UIStyler.StylerItem
Represents a Real for UI Styler
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
ItemValue | Returns or sets the item value |
Sensitivity | Returns or sets the sensitivity |
Visibility | Returns or sets the visibility |
Methods¶
Method | Description |
---|---|
AddActivateHandler | Registers activate callback. |
Dispose | Free resources associated with the instance. |
GetItemType | Gets the dialog item type. |
InitializeAttachment | Returns initialized dialog item attachment information @return attachment object |
IsEqualTo | Equates two styler items @return |
SetAttachment | Specifies the updated dialog item attachment information |
SetBitmap | |
SetFocus | Sets focus |
SetLabel | Set the label |
Property Detail¶
ItemValue¶
-
RealItem.
ItemValue
¶ Returns or sets the item value
-------------------------------------
Getter Method
Signature
ItemValue()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ItemValue(itemVal)
Parameters: itemVal (float) – Real value to display in the text field New in version NX5.0.0.
License requirements: None.
Sensitivity¶
-
RealItem.
Sensitivity
¶ Returns or sets the sensitivity
-------------------------------------
Getter Method
Signature
Sensitivity()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Sensitivity(type)
Parameters: type (bool) – TRUE if sensitive, FALSE if insensitive New in version NX5.0.0.
License requirements: None.
Visibility¶
-
RealItem.
Visibility
¶ Returns or sets the visibility
-------------------------------------
Getter Method
Signature
Visibility()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Visibility(type)
Parameters: type (bool) – TRUE if visible, FALSE if invisible New in version NX5.0.0.
License requirements: None.
Method Detail¶
AddActivateHandler¶
-
RealItem.
AddActivateHandler
¶ Registers activate callback.
This method should be called before calling
UIStyler.Dialog.Show()
orUIStyler.Dialog.RegisterWithUiMenu()
Signature
AddActivateHandler(activateevent, isDialogLaunchingEvent)
Parameters: - activateevent (CallableObject) – Callback for activate event
- isDialogLaunchingEvent (bool) – TRUE if dialog is going to launch, FALSE if not
New in version NX5.0.0.
License requirements: None.
SetBitmap¶
-
RealItem.
SetBitmap
¶ Signature
SetBitmap(strBitmap)
Parameters: strBitmap (str) – Filename with .ubm, .xpm, or .bmp extension that contains a bitmap definition New in version NX5.0.0.
License requirements: None.