PropertyPage Class¶
-
class
NXOpen.UIStyler.
PropertyPage
¶ Bases:
NXOpen.UIStyler.StylerItem
Represents a PropertyPage for UI Styler
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Sensitivity | Returns or sets the sensitivity of property page. |
Visibility | Returns or sets the visibility of the dialog item. |
Methods¶
Method | Description |
---|---|
Dispose | Free resources associated with the instance. |
GetItemType | Gets the dialog item type. |
InitializeAttachment | Returns initialized dialog item attachment information @return attachment object |
IsEqualTo | Equates two styler items @return |
SetAttachment | Specifies the updated dialog item attachment information |
SetFocus | Sets focus |
SetLabel | Specifies descriptive text to display for the dialog item. |
Property Detail¶
Sensitivity¶
-
PropertyPage.
Sensitivity
¶ Returns or sets the sensitivity of property page.
-------------------------------------
Getter Method
Signature
Sensitivity()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Sensitivity(type)
Parameters: type (bool) – New in version NX5.0.0.
License requirements: None.
Visibility¶
-
PropertyPage.
Visibility
¶ Returns or sets the visibility of the dialog item.
-------------------------------------
Getter Method
Signature
Visibility()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Visibility(type)
Parameters: type (bool) – New in version NX5.0.0.
License requirements: None.
Method Detail¶
SetFocus¶
-
PropertyPage.
SetFocus
¶ Sets focus
Signature
SetFocus()
New in version NX5.0.0.
License requirements: None.
SetLabel¶
-
PropertyPage.
SetLabel
¶ Specifies descriptive text to display for the dialog item.
It should describe the dialog item’s intended use. If you specify a bitmap for this dialog item, it uses this text as tooltip text.
Signature
SetLabel(strLabel)
Parameters: strLabel (str) – new label New in version NX5.0.0.
License requirements: None.