OptionToggle Class¶
-
class
NXOpen.UIStyler.
OptionToggle
¶ Bases:
NXOpen.UIStyler.StylerItem
Represents a OptionToggle for UI Styler
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Visibility | Returns or sets the visibility |
Methods¶
Method | Description |
---|---|
AddActivateHandler | Registers activate callback. |
AddValueChangedHandler | Registers value change callback. |
Dispose | Free resources associated with the instance. |
GetItemType | Gets the dialog item type. |
GetItemValue | Returns item value @return Item value |
GetItems | Returns the items @return An array of items |
GetSensitivity | Returns the sesitivity @return |
InitializeAttachment | Returns initialized dialog item attachment information @return attachment object |
IsEqualTo | Equates two styler items @return |
SetAttachment | Specifies the updated dialog item attachment information |
SetBitmaps | Set bitmaps |
SetDefaultAction | Sets default action |
SetItemValue | Sets item value |
SetItems | Sets items in the array |
SetLabel | Sets label |
SetSensitivity | Set the sesitivity |
Property Detail¶
Visibility¶
-
OptionToggle.
Visibility
¶ Returns or sets the visibility
-------------------------------------
Getter Method
Signature
Visibility()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Visibility(type)
Parameters: type (bool) – TRUE if visible, FALSE if invisible New in version NX5.0.0.
License requirements: None.
Method Detail¶
AddActivateHandler¶
-
OptionToggle.
AddActivateHandler
¶ Registers activate callback.
This method should be called before calling
UIStyler.Dialog.Show()
orUIStyler.Dialog.RegisterWithUiMenu()
Signature
AddActivateHandler(activateevent, isDialogLaunchingEvent)
Parameters: - activateevent (CallableObject) – Callback for activate event
- isDialogLaunchingEvent (bool) – TRUE if dialog is going to launch, FALSE if not
New in version NX5.0.0.
License requirements: None.
AddValueChangedHandler¶
-
OptionToggle.
AddValueChangedHandler
¶ Registers value change callback.
This method should be called before calling
UIStyler.Dialog.Show()
orUIStyler.Dialog.RegisterWithUiMenu()
Signature
AddValueChangedHandler(valuechangedevent, isDialogLaunchingEvent)
Parameters: - valuechangedevent (CallableObject) – Callback for value changed event
- isDialogLaunchingEvent (bool) – TRUE if dialog is going to launch, FALSE if not
New in version NX5.0.0.
License requirements: None.
GetItemValue¶
-
OptionToggle.
GetItemValue
¶ Returns item value
Signature
GetItemValue()
Returns: a tuple Return type: A tuple consisting of (itemVal, setCheck). itemVal is a int. Item value setCheck is a bool. New in version NX5.0.0.
License requirements: None.
GetItems¶
-
OptionToggle.
GetItems
¶ Returns the items
Signature
GetItems()
Returns: An array of items Return type: list of str New in version NX5.0.0.
License requirements: None.
GetSensitivity¶
-
OptionToggle.
GetSensitivity
¶ Returns the sesitivity
Signature
GetSensitivity()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
SetBitmaps¶
-
OptionToggle.
SetBitmaps
¶ Set bitmaps
Signature
SetBitmaps(bitmaps)
Parameters: bitmaps (list of str) – An array of one or more bitmap filenames. If all bitmaps for the option menu reside in the same file, specify an array of just one entry, which contains the bitmap filename for this attribute. All existing choices for the option menu remain intact when this attribute is set. Only the bitmaps are changed. Note that the number of bitmaps must match the number of existing choices. New in version NX5.0.0.
License requirements: None.
SetDefaultAction¶
-
OptionToggle.
SetDefaultAction
¶ Sets default action
Signature
SetDefaultAction()
New in version NX5.0.0.
License requirements: None.
SetItemValue¶
-
OptionToggle.
SetItemValue
¶ Sets item value
Signature
SetItemValue(subitemIndex, setCheck)
Parameters: - subitemIndex (int) – Zero-based index indicating the choice to be selected. It must be in the range of existing choices.
- setCheck (bool) – TRUE if set, FALSE if unset.
New in version NX5.0.0.
License requirements: None.
SetItems¶
-
OptionToggle.
SetItems
¶ Sets items in the array
Signature
SetItems(strListArray)
Parameters: strListArray (list of str) – An array of new choices to be used for the dialog item. Note that this removes all existing choices (both text and bitmaps). New in version NX5.0.0.
License requirements: None.
SetLabel¶
-
OptionToggle.
SetLabel
¶ Sets label
Signature
SetLabel(strLabel)
Parameters: strLabel (str) – Text to be set for the tool tip. New in version NX5.0.0.
License requirements: None.
SetSensitivity¶
-
OptionToggle.
SetSensitivity
¶ Set the sesitivity
Signature
SetSensitivity(subitemIndex, type)
Parameters: - subitemIndex (int) – If the entire dialog item should change to the new Sensitivity state, set this field to UF_STYLER_NO_SUB_INDEX. If only one sub-item should change to the new sensitivity state, set this field to its zero-based index.
- type (bool) – TRUE if sensitive, FALSE if insensitive
New in version NX5.0.0.
License requirements: None.