MultiTextBox Class¶
-
class
NXOpen.UIStyler.
MultiTextBox
¶ Bases:
NXOpen.UIStyler.StylerItem
Represents a MultiTextBox for UI Styler.
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Sensitivity | Returns or sets the sensitivity of the dialog item. |
Visibility | Returns or sets the visibility of the dialog item |
Methods¶
Method | Description |
---|---|
Dispose | Free resources associated with the instance. |
GetItemType | Gets the dialog item type. |
GetItemValues | Specifies the text for this dialog item. |
InitializeAttachment | Returns initialized dialog item attachment information @return attachment object |
IsEqualTo | Equates two styler items @return |
SetAttachment | Specifies the updated dialog item attachment information |
SetFocus | Indicates that this dialog item is receiving keyboard focus. |
SetItemValues | Specifies the text for this dialog item. |
SetLabel | Specifies descriptive text to display for the dialog item. |
Property Detail¶
Sensitivity¶
-
MultiTextBox.
Sensitivity
¶ Returns or sets the sensitivity of the dialog item.
-------------------------------------
Getter Method
Signature
Sensitivity()
Returns: to get senstivity of dialog Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Sensitivity(type)
Parameters: type (bool) – to set senstivity of dialog New in version NX5.0.0.
License requirements: None.
Visibility¶
-
MultiTextBox.
Visibility
¶ Returns or sets the visibility of the dialog item
-------------------------------------
Getter Method
Signature
Visibility()
Returns: to get visibility of dialog Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Visibility(type)
Parameters: type (bool) – to set visibility of dialog New in version NX5.0.0.
License requirements: None.
Method Detail¶
GetItemValues¶
-
MultiTextBox.
GetItemValues
¶ Specifies the text for this dialog item.
It can be programmatically get by APIs.
Signature
GetItemValues()
Returns: to get array of strings Return type: list of str New in version NX5.0.0.
License requirements: None.
SetFocus¶
-
MultiTextBox.
SetFocus
¶ Indicates that this dialog item is receiving keyboard focus.
Signature
SetFocus()
New in version NX5.0.0.
License requirements: None.
SetItemValues¶
-
MultiTextBox.
SetItemValues
¶ Specifies the text for this dialog item.
It can be programmatically set by APIs supported in different laguages,or interactively entered by the user.
Signature
SetItemValues(values)
Parameters: values (list of str) – array of strings to set the values in multi select List New in version NX5.0.0.
License requirements: None.