FileOperationDataFileOperationType Enumeration

NXOpen.UIStyler.FileOperationData.FileOperationType is an alias for NXOpen.UIStyler.FileOperationDataFileOperationType

class NXOpen.UIStyler.FileOperationDataFileOperationType

Bases: object

Describes file operation

Enum Members

Enum Member Enum Member Description
New
New file operation
Open
Open file operation
Save
Save file operation
SaveAs
Save as file operation
SaveAll
Save all file operation
Close
Close file operation
Quit
Quit file operation
SaveAndExit
Save and Exit file operation
ChangePart
Chaneg part file operation
Execute
Execute file operation
Reopen
Reopen file operation
SaveAllAndClose
Save all and close file operation
SaveAndClose
Save and close file operation
SaveAsAndClose
Save as and close file operation
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.