FileOperationDataFileOperationState Enumeration

NXOpen.UIStyler.FileOperationData.FileOperationState is an alias for NXOpen.UIStyler.FileOperationDataFileOperationState

class NXOpen.UIStyler.FileOperationDataFileOperationState

Bases: object

Describes file state

Enum Members

Enum Member Enum Member Description
Enter
Enter file state
Exit
Exit file state
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.