DialogState Enumeration

class NXOpen.UIStyler.DialogState

Bases: object

Represents the dialog state Enum Members

Enum Member Enum Member Description
ContinueDialog
Continue the dialog
ExitDialog
Exit from the dialog
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.