DialogResponse Enumeration¶
-
class
NXOpen.UIStyler.
DialogResponse
¶ Bases:
object
Represents dialog response Enum Members
Enum Member Enum Member Description PickResponse User response was a selection of objects.Ok OK button was selected.Cancel Cancel button was selected.Back Back button was selected.Apply Apply button was selected.Help Help button was selected.ObjectSelected Object was selected.ObjectSelectedByName Object was selected by name.CbTerminate Callback routine has terminated.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-