ColorTool Class¶
-
class
NXOpen.UIStyler.
ColorTool
¶ Bases:
NXOpen.UIStyler.StylerItem
Represents a ColorTool for UI Styler.
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
ItemValue | Returns or sets the item value |
Sensitivity | Returns or sets the sensitivity |
Visibility | Returns or sets the visibility |
Methods¶
Method | Description |
---|---|
AddValueChangedHandler | Registers value change callback. |
Dispose | Free resources associated with the instance. |
GetItemType | Gets the dialog item type. |
InitializeAttachment | Returns initialized dialog item attachment information @return attachment object |
IsEqualTo | Equates two styler items @return |
SetAttachment | Specifies the updated dialog item attachment information |
Property Detail¶
ItemValue¶
-
ColorTool.
ItemValue
¶ Returns or sets the item value
-------------------------------------
Getter Method
Signature
ItemValue()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ItemValue(itemVal)
Parameters: itemVal (int) – Integer value to display in the text field New in version NX5.0.0.
License requirements: None.
Sensitivity¶
-
ColorTool.
Sensitivity
¶ Returns or sets the sensitivity
-------------------------------------
Getter Method
Signature
Sensitivity()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Sensitivity(type)
Parameters: type (bool) – TRUE if sensitive, FALSE if insensitive New in version NX5.0.0.
License requirements: None.
Visibility¶
-
ColorTool.
Visibility
¶ Returns or sets the visibility
-------------------------------------
Getter Method
Signature
Visibility()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Visibility(type)
Parameters: type (bool) – TRUE if visible, FALSE if invisible New in version NX5.0.0.
License requirements: None.
Method Detail¶
AddValueChangedHandler¶
-
ColorTool.
AddValueChangedHandler
¶ Registers value change callback.
This method should be called before calling
UIStyler.Dialog.Show()
orUIStyler.Dialog.RegisterWithUiMenu()
Signature
AddValueChangedHandler(valuechangedevent, isDialogLaunchingEvent)
Parameters: - valuechangedevent (CallableObject) – Callback for value changed event
- isDialogLaunchingEvent (bool) – TRUE if dialog is going to launch, FALSE if not
New in version NX5.0.0.
License requirements: None.