NXOpen.UF.Wave.SetLinkedPtPoint¶
-
Wave.
SetLinkedPtPoint
()¶ Refer to UF_WAVE_set_linked_pt_point for documentation.
Signature:
SetLinkedPtPoint(linkedFeature, point, xform)
Parameters: - linkedFeature (Tag) – The linked point feature whose properties are to be set.
- point (Tag) – The point which is the new source geometry of the linked point feature; can be NULL_TAG, in which case the link is broken.
- xform (Tag) – The new transform which determines the position of the linked point feature relative to its source geometry. Must be NULL_TAG or an assy_ctxt_xform in the same part as linked_feature whose to_part_occ contains point.
License requirements: SOLIDS MODELING