NXOpen.UF.Wave.SetLinkedPtCenter¶
-
Wave.
SetLinkedPtCenter
()¶ Refer to UF_WAVE_set_linked_pt_center for documentation.
Signature:
SetLinkedPtCenter(linkedFeature, conic, xform)
Parameters: - linkedFeature (Tag) – The linked point feature whose properties are to be set.
- conic (Tag) – The conic whose center is the new source geometry of the linked point feature.
- xform (Tag) – The new transform which determines the position of the linked point feature relative to its source geometry. Must be NULL_TAG or an assy_ctxt_xform in the same part as linked_feature whose to_part_occ contains conic.
License requirements: SOLIDS MODELING