NXOpen.UF.Wave.SetLinkedPtAngle¶
-
Wave.
SetLinkedPtAngle
()¶ Refer to UF_WAVE_set_linked_pt_angle for documentation.
Signature:
SetLinkedPtAngle(linkedFeature, arc, angle, xform)
Parameters: - linkedFeature (Tag) – The linked point feature whose properties are to be set.
- arc (Tag) – The arc which defines the new source geometry of the linked point feature.
- angle (Tag) – The angle (smart scalar) which defines the position of the linked point feature around arc. It must be in the same part as linked_feature. Its value is in radians.
- xform (Tag) – The new transform which determines the position of the linked point feature relative to its source geometry. Must be NULL_TAG (identity transform) or an assy_ctxt_xform in the same part as linked_feature whose to_part_occ contains arc.
License requirements: SOLIDS MODELING