NXOpen.UF.Wave.SetLinkData¶
-
Wave.
SetLinkData
()¶ Refer to UF_WAVE_set_link_data for documentation.
Signature:
SetLinkData(linkedFeature, sourceEntity, xform, updateAtTimestamp)
Parameters: - linkedFeature (Tag) – The linked feature whose properties are to be set.
- sourceEntity (Tag) – The tag of the new source geometry; can be NULL_TAG, in which case the link is broken.
- xform (Tag) – The new transform which determines the position of the linked feature relative to its source geometry. Must be NULL_TAG (identity transform) or an assy_ctxt_xform in the same part as linked_feature whose to_part_occ contains source_entity.
- updateAtTimestamp (bool) – If true, the linked feature now updates at its timestamp. If false, the feature now updates after its source geometry has updated.
License requirements: None