NXOpen.UF.Wave.LoadParents¶
-
Wave.
LoadParents
()¶ Refer to UF_WAVE_load_parents for documentation.
Signature:
LoadParents(part, parentOption)
Parameters: - part (Tag) – Tag of the part for which to load the parts of
- parentOption (int) – This is the WAVE load option as described in uf_assem_types.h UF_ASSEM_none Don’t load any non-loaded parents, but fully load partially loaded parents. UF_ASSEM_immediate Only load the immediate parents (First-level parents) UF_ASSEM_all Recursively load parents, and parents of parents until there are no more parents left to load.
Returns: A Tuple
Return type: A tuple consisting of (nFailures,failingParts,failingStatuses,int)
nFailures(int): Number of parent parts that failed to load
failingParts(list of str): Names of the parts that failed to load Use UF_free_string_array to deallocate memory when done.
failingStatuses(list of int): Error codes for the failures in corresponding order Use UF_free to deallocate memory when done.
retVar(int):
License requirements: WAVE FUNCTIONALITY