NXOpen.UF.Wave.CreateLinkedString¶
-
Wave.
CreateLinkedString
()¶ Refer to UF_WAVE_create_linked_string for documentation.
Signature:
CreateLinkedString(string, xform, objectInPart)
Parameters: - string (Tag) – The string feature whose curves are the source geometry of the new linked string feature.
- xform (Tag) – The transform which determines the position of the linked feature relative to its source geometry. Must be NULL_TAG (create position independent link) or an assy_ctxt_xform in the same part as object_in_part whose to_part_occ contains string. Linked strings must be interpart.
- objectInPart (Tag) – Determines the part within which the new feature is made.
Returns: The tag of the new linked string feature.
Return type: License requirements: ASSEMBLIES MODULE