NXOpen.UF.Wave.CreateLinkedSketch¶
-
Wave.
CreateLinkedSketch
()¶ Refer to UF_WAVE_create_linked_sketch for documentation.
Signature:
CreateLinkedSketch(sketch, xform, objectInPart)
Parameters: - sketch (Tag) – The sketch which is the source geometry of the new linked sketch feature.
- xform (Tag) – The transform which determines the position of the linked feature relative to its source geometry. Must be NULL_TAG (create position independent link) or an assy_ctxt_xform in the same part as object_in_part whose to_part_occ contains sketch. Linked sketches must be interpart.
- objectInPart (Tag) – Determines the part within which the new feature is made.
Returns: The tag of the new linked sketch feature.
Return type: License requirements: ASSEMBLIES MODULE