NXOpen.UF.Wave.CreateLinkedRouteSegment¶
-
Wave.
CreateLinkedRouteSegment
()¶ Refer to UF_WAVE_create_linked_route_segment for documentation.
Signature:
CreateLinkedRouteSegment(segment, xform, objectInPart)
Parameters: - segment (Tag) – The segment which is the source geometry of the new linked segment.
- xform (Tag) – The transform which determines the position of the linked object relative to its source geometry. Must be NULL_TAG (apply no transformation) or an assy_ctxt_xform in the same part as object_in_part whose to_part_occ contains curve.
- objectInPart (Tag) – Determines the part within which the new linked segment copy is made.
Returns: A Tuple
Return type: A tuple consisting of (linkedCurveFeature,linkedSegment)
linkedCurveFeature(Tag): The tag of the LINKED_CURVE feature which the linked segment follows.
linkedSegment(Tag): The tag of the segment that follows the LINKED_CURVE
License requirements: ASSEMBLIES MODULE