NXOpen.UF.Wave.CreateLinkedRoutePort¶
-
Wave.
CreateLinkedRoutePort
()¶ Refer to UF_WAVE_create_linked_route_port for documentation.
Signature:
CreateLinkedRoutePort(port, xform, objectInPart)
Parameters: - port (Tag) – The port which is the source geometry of the new linked port.
- xform (Tag) – The transform which determines the position of the linked object relative to its source geometry. Must be NULL_TAG (apply no transformation) or an assy_ctxt_xform in the same part as object_in_part whose to_part_occ contains curve.
- objectInPart (Tag) – Determines the part within which the new linked port copy is made.
Returns: The tag of the new linked port feature.
Return type: License requirements: ASSEMBLIES MODULE