NXOpen.UF.Wave.CreateLinkedPtPoint¶
-
Wave.
CreateLinkedPtPoint
()¶ Refer to UF_WAVE_create_linked_pt_point for documentation.
Signature:
CreateLinkedPtPoint(point, xform, objectInPart)
Parameters: - point (Tag) – The point which is the source geometry of the new linked point feature.
- xform (Tag) – Gives the transformation that is applied to the source point to generate the linked point. It must be NULL_TAG (create position independent link) or an assy_ctxt_xform in the same part as object_in_part whose to_part_occ contains point.
- objectInPart (Tag) – Determines the part within which the new feature is made.
Returns: The tag of the new linked point feature.
Return type: License requirements: ASSEMBLIES MODULE