NXOpen.UF.Wave.CreateLinkedMirror¶
-
Wave.
CreateLinkedMirror
()¶ Refer to UF_WAVE_create_linked_mirror for documentation.
Signature:
CreateLinkedMirror(body, bodyXform, datumPlane, datumXform, objectInPart, updateAtTimestamp)
Parameters: - body (Tag) – The body which is the source geometry of the new linked mirror body feature.
- bodyXform (Tag) – The transform which determines the position of the linked feature relative to its source body, before the reflection is applied. Must be NULL_TAG (apply no transformation) or an assy_ctxt_xform in the same part as object_in_part whose to_part_occ contains body.
- datumPlane (Tag) – The datum plane which provides the plane of reflection of the new linked mirror body feature.
- datumXform (Tag) – The transform which determines the position of the plane of reflection of the linked feature relative to its source datum plane. Must be NULL_TAG (apply no transformation) or an assy_ctxt_xform whose to_part_occ contains datum_plane.
- objectInPart (Tag) – Determines the part within which the new feature is made.
- updateAtTimestamp (bool) – If true, the feature updates at its creation timestamp. If false, the feature updates after its source geometry is completely generated.
Returns: The tag of the new linked mirror feature.
Return type: License requirements: ASSEMBLIES MODULE