NXOpen.UF.Wave.CreateLinkedCurve¶
-
Wave.
CreateLinkedCurve
()¶ Refer to UF_WAVE_create_linked_curve for documentation.
Signature:
CreateLinkedCurve(curve, xform, objectInPart, updateAtTimestamp)
Parameters: - curve (Tag) – The curve which is the source geometry of the new linked curve feature.
- xform (Tag) – The transform which determines the position of the linked feature relative to its source geometry. Must be NULL_TAG (create position independent link) or an assy_ctxt_xform in the same part as object_in_part whose to_part_occ contains curve.
- objectInPart (Tag) – Determines the part within which the new feature is made.
- updateAtTimestamp (bool) – If true, the linked curve feature updates at a time determined by its creation timestamp. If it is false, it updates after its source curve is completely generated.
Returns: The tag of the new linked curve feature.
Return type: License requirements: ASSEMBLIES MODULE