NXOpen.UF.Wave.CopyComponentAs¶
-
Wave.
CopyComponentAs
()¶ Refer to UF_WAVE_copy_component_as for documentation.
Signature:
CopyComponentAs(sourcePartOccurrence, sourcePartName, newPartName, referenceSetName, instanceName, transform)
Parameters: - sourcePartOccurrence (Tag) – The part occurrence that is being copied
- sourcePartName (str) – The component part name that is to be copied
- newPartName (str) – The new component part name that will exist in the current assembly.
- referenceSetName (str) – Name of reference set to use from component parts. The refset_name cannot exceed 30 characters, cannot include a directory path, and should not have a file extension.
- instanceName (str) – Name of new instance The instance_name cannot exceed 30 characters, cannot include a directory path, and should not have a file extension.
- transform (list of float) – The transform to apply to the new component
Returns: A Tuple
Return type: A tuple consisting of (newInstance,newPart)
newInstance(Tag): The new instance tag created in the assembly
newPart(Tag): The new part tag that is a copy of parent part.
License requirements: WAVE FUNCTIONALITY