NXOpen.UF.Wave.AskLinkRegionSources¶
-
Wave.
AskLinkRegionSources
()¶ Refer to UF_WAVE_ask_link_region_sources for documentation.
Signature:
AskLinkRegionSources(linkedFeature, allowLoad)
Parameters: - linkedFeature (Tag) – The linked region feature whose source geometry is wanted.
- allowLoad (bool) – True if the source geometry’s part can be loaded, false otherwise.
Returns: A Tuple
Return type: A tuple consisting of (nSeedFaces,seedFaces,nBoundaryFaces,boundaryFaces,traverseInteriorEdges,deleteOpenings)
nSeedFaces(int): The number of seed faces.
seedFaces(list of Tag): The array of tags of the seed faces. This must be freed by calling UF_free.
nBoundaryFaces(int): The number of boundary faces.
boundaryFaces(list of Tag): The array of tags of the boundary faces. This must be freed by calling UF_free.
traverseInteriorEdges(bool): True if the traversal algorithm passes through holes in the body; false if it only passes over the outside surface of the body.
deleteOpenings(bool): True if any holes in the resulting sheet are closed up; false if they are left.
License requirements: None