NXOpen.UF.Wave.AskLinkMirrorData¶
-
Wave.
AskLinkMirrorData
()¶ Refer to UF_WAVE_ask_link_mirror_data for documentation.
Signature:
AskLinkMirrorData(linkedFeature, allowLoad)
Parameters: - linkedFeature (Tag) – The linked mirror feature whose source geometry and xforms are wanted.
- allowLoad (bool) – True if the source geometry’s part can be loaded, false otherwise.
Returns: A Tuple
Return type: A tuple consisting of (sourceBody,bodyXform,datumPlane,datumXform)
sourceBody(Tag): The body which is the source geometry of the linked mirror body feature.
bodyXform(Tag): The transform which determines the position of the linked feature relative to its source body.
datumPlane(Tag): The datum plane which provides the plane of reflection of the linked mirror body feature.
datumXform(Tag): The transform which determines the position of the plane of reflection of the linked feature relative to its source datum plane.
License requirements: None