NXOpen.UF.View.Visualization Structure¶
NXOpen.UF.View.Visualization is an alias for NXOpen.UF.ViewVisualization_Struct
-
class
NXOpen.UF.
ViewVisualization_Struct
¶ Bases:
object
Refer to UF_VIEW_visualization_s for documentation.
Fields
NXOpen.UF.ViewVisualization_Struct.DisplayMode |
Display mode for the view. |
NXOpen.UF.ViewVisualization_Struct.HiddenEdgeMode |
Hidden edge style for the view The following constants are valid : UF_VIEW_HIDDEN_EDGES_SOLID, UF_VIEW_HIDDEN_EDGES_INVIS, UF_VIEW_HIDDEN_EDGES_DASHED, UF_VIEW_HIDDEN_SURFACE and UF_VIEW_HIDDEN_EDGES_GRAY_THIN |
NXOpen.UF.ViewVisualization_Struct.SilhouetteMode |
Silhouettes flag (on or off) in the view The following constants are valid : UF_VIEW_SILHOUETTES_ON and UF_VIEW_SILHOUETTES_OFF |
NXOpen.UF.ViewVisualization_Struct.SmoothEdgesMode |
Smooth edges flag (on or off) in the view The following constants are valid : UF_VIEW_SMOOTH_EDGES_ON and UF_VIEW_SMOOTH_EDGES_OFF |
NXOpen.UF.ViewVisualization_Struct.SmoothEdgeColor |
Smooth edges color in the view The following values are valid : UF_OBJ_COLOR_ORIGINAL, [ 1 - 216 ] |
NXOpen.UF.ViewVisualization_Struct.SmoothEdgeFont |
Smooth edges font in the view The following constants are valid : UF_OBJ_FONT_ORIGINAL, UF_OBJ_FONT_SOLID, UF_OBJ_FONT_DASHED, UF_OBJ_FONT_PHANTOM, UF_OBJ_FONT_CENTERLINE, UF_OBJ_FONT_DOTTED, UF_OBJ_FONT_LONG_DASHED and UF_OBJ_FONT_DOTTED_DASHED |
NXOpen.UF.ViewVisualization_Struct.SmoothEdgeWidth |
Smooth edges width in the view The following constants are valid : UF_OBJ_WIDTH_ORIGINAL, UF_OBJ_WIDTH_THIN, UF_OBJ_WIDTH_NORMAL and UF_OBJ_WIDTH_THICK |
NXOpen.UF.ViewVisualization_Struct.SmoothEdgeAngleTolerance |
Smooth edge angle tolerance in the view. |
NXOpen.UF.ViewVisualization_Struct.FogMode |
Fog mode in viewThe following constants are valid : UF_VIEW_FOG_OFF, UF_VIEW_FOG_LINEAR, UF_VIEW_FOG_LIGHT and UF_VIEW_FOG_HEAVY |
NXOpen.UF.ViewVisualization_Struct.FogColor |
Fog color[0] = red, [1] = green, [2] = blue Each color has a range from 0.0 to 1.0. |
NXOpen.UF.ViewVisualization_Struct.FogFront |
Front fog plane has a range from 0 to 100 and is only valid for fog_mode = UF_VIEW_FOG_LINEAR |
NXOpen.UF.ViewVisualization_Struct.FogBack |
Back fog plane has a range from 0 to 100 and is only valid for fog_mode = UF_VIEW_FOG_LINEAR. |
NXOpen.UF.ViewVisualization_Struct.FogRate |
The fog density which has a range from 0 to 100. |