NXOpen.UF.Ui.SelectPointCollection¶
-
Ui.
SelectPointCollection
()¶ Refer to UF_UI_select_point_collection for documentation.
Signature:
SelectPointCollection(message, coincidentPoints)
Parameters: - message (str) – Displays a message (32 character maximum) in the cue line. The message is suffixed with the string “Point Specification Method”.
- coincidentPoints (bool) – TRUE = coincident points can be returned. FALSE = do not return coincident points. not valid with point constructor
Returns: A Tuple
Return type: A tuple consisting of (points,count,response)
points(list of ``NXOpen.UF.Ui.ChainedPoints` Refer to UF_UI_chained_points_s for documentation.`): Array of data structures containing the points. This array must be freed by calling UF_free.
count(int): Count of points returned.
response(int): A response of Back, Cancel , or OK is specified by one of the following constants: UF_UI_BACK UF_UI_CANCEL UF_UI_OK
License requirements: None