NXOpen.UF.Ui.PointConstruct¶
-
Ui.
PointConstruct
()¶ Refer to UF_UI_point_construct for documentation.
Signature:
PointConstruct(cue, baseMethod)
Parameters: - cue (str) – Displays a message in the cue line.
- baseMethod (
NXOpen.UF.Ui.PointBaseMethod
Refer to UF_UI_point_base_method_e for documentation.) – Use this method as the default method. Returns the method used to create the point.
Returns: A Tuple
Return type: A tuple consisting of (baseMethod,pointTag,basePt,response)
baseMethod(
`NXOpen.UF.Ui.PointBaseMethod
Refer to UF_UI_point_base_method_e for documentation.`): Modified value of baseMethodpointTag(Tag): Constructed point. The point is an associative (SO) point that is invisible by default. Use UF_SO_set_visibility_option to make it visible. Use functions in uf_so.h to query the parents. See information above in the description about circumstances that will cause a non-associative point to be returned. NULL_TAG is returned if dialog is terminated with CANCEL.
basePt(list of float): Coordinates of created point, in absolute work part coordinates.
response(int): One of the following: UF_UI_OK UF_UI_BACK UF_UI_CANCEL.
License requirements: None