NXOpen.UF.Ui.GetInputIntegers¶
-
Ui.
GetInputIntegers
()¶ Refer to UF_UI_get_input_integers for documentation.
Signature:
GetInputIntegers(cp1, cp2, ip3, ia4, ip5)
Parameters: - cp1 (str) – The message to display on the cue line, a maximum of 80 characters.
- cp2 (list of str) – The menu list.
- ip3 (int) – The number of items in the menu list, cp2, this must be less than or equal to 14.
- ia4 (list of int) – On input the initial parameter values. On output the modified parameter values. This should be an array with ip3 entries. These will be the values the user can modify.
- ip5 (int) – Unused.
Returns: A Tuple
Return type: A tuple consisting of (ia4,int)
ia4(list of int): Modified value of ia4
retVar(int): 1 = Back2 = Cancel Operation3 = OK - No user input4 = OK with user input8 = Disallowed state, unable to bring up dialogSee Also:History:
License requirements: None