NXOpen.UF.Ui.GetInputDoubles¶
-
Ui.
GetInputDoubles
()¶ Refer to UF_UI_get_input_doubles for documentation.
Signature:
GetInputDoubles(cp1, cp2, ip3, ra4, ip5)
Parameters: - cp1 (str) – Menu title displayed on the cue line. This may be a maximum of 80 characters.
- cp2 (list of str) – This is the array of menu items to display.
- ip3 (int) – This is the number of items in the menu array, cp2. This is also the size of the double arrays.
- ra4 (list of float) – On input these are the initial parameter values. On output these are the values as modified by the user. This must be an array dimensioned to [ip3].
- ip5 (int) – Unused
Returns: A Tuple
Return type: A tuple consisting of (ra4,int)
ra4(list of float): Modified value of ra4
retVar(int): 1 = Back2 = Cancel Operation3 = OK - No user input4 = OK with user input8 = Disallowed state, unable to bring up dialogSee Also:History:
License requirements: None