NXOpen.UF.Ui.DisplayMultiSelectMenu¶
-
Ui.
DisplayMultiSelectMenu
()¶ Refer to UF_UI_display_multi_select_menu for documentation.
Signature:
DisplayMultiSelectMenu(cue, ip2, items, numItems)
Parameters: - cue (str) – Menu title to display on the cue line. This is 80 characters maximum.
- ip2 (int) – Unused.
- items (list of str) – String array containing the menu items.
- numItems (int) – Number of strings in the cp3 array. This may not exceed 14 menu items.
Returns: A Tuple
Return type: A tuple consisting of (selected,int)
selected(list of int): Selection Array, which should be dimensioned to num_items. if ir6[n] == 0, then cp3[n][38] was not selected. if ir6[n] == 1, then cp3[n][38] was selected.
retVar(int): 1 = Back2 = Cancel Operation3 = OK4 = Alternate Action8 = Disallowed state, unable to bring up dialogSee Also:History:
License requirements: None