NXOpen.UF.Ui.AskStringInput¶
-
Ui.
AskStringInput
()¶ Refer to UF_UI_ask_string_input for documentation.
Signature:
AskStringInput(cue, str)
Parameters: - cue (str) – Menu title (displayed on the cue line, maximum of 80 characters.
- str (list of str) – On input the default value of the string, on output the string typed in. This should be declared as char str[133] in the calling program.
Returns: A Tuple
Return type: A tuple consisting of (str,length,int)
str(list of str): Modified value of str
length(int): The length of the returned string in ca2.
retVar(int): 1 = Back2 = Cancel3 = OK (Accept default )5 = Data entered8 = Disallowed state, unable to bring up dialogSee Also:History:
License requirements: None