NXOpen.UF.Ui.AskCreatePartFilename¶
-
Ui.
AskCreatePartFilename
()¶ Refer to UF_UI_ask_create_part_filename for documentation.
Signature:
AskCreatePartFilename(fileName, units)
Parameters: - fileName (list of str) – On input default file name to use for part creation dialog. On output the filename actually used.
- units (int) – On input default units to use for part creation dialog. On output the units actually used. UF_PART_METRIC UF_PART_ENGLISH NONE = uses default
Returns: A Tuple
Return type: A tuple consisting of (fileName,units,response)
fileName(list of str): Modified value of fileName
units(int): Modified value of units
response(int): User response from dialog: UF_UI_OK UF_UI_CANCEL
License requirements: None